Teamcenter Oracle CPU for January 2023 is Available

2023-02-20T15:53:53Z
Reporting and Analytics

Summary


Details

Oracle has released a quarterly Critical Patch Update to fix vulnerabilities in Oracle database products: Oracle Critical Patch Update for January 2023 .

These patches are available for download by licensed customers at https://support.sw.siemens.com  

  • Go to Support Center and choose the Oracle Product. 
    • Click on Downloads, then choose from the 'Select a Version' drop down.
      • To access the latest Opatch installers, choose the Version and Opatch from the 'Select a Version' drop down.

        The patches include:

        Oracle 19c (19.18.0.0.230117)

           p34765931_190000_Linux-x86-64.zip

           p34750795_190000_MSWIN-x86-64.zip    

        Oracle 19c Opatch (12.2.0.1.36)

           p6880880_190000_Linux-x86-64.zip  

          p6880880_190000_MSWIN-x86-64.zip 

          p6880880_190000_Solaris-x86-64.zip

        Teamcenter supports these versions of Oracle Database: 

            For the latest information, please refer to the Teamcenter Platform Matrix

            at Support Center.  It is located under Support White Papers under Teamcenter

            Download.

            Oracle 12c - Teamcenter 10.1.5, Teamcenter 11.x, Teamcenter 12.x

            Oracle 18c - Teamcenter 11.x, Teamcenter 12.x

            Oracle 19c - Teamcenter 12.4.x, Teamcenter 13.x, Teamcenter 14.x

         

        Note1: Oracle 12.1.0.x is out of support as of 19-Jul-2019 and no additional patches are

                 posted for this version.

        Note2: Oracle 18c is out of support as of 30-Jun-2021 and no additional patches are posted 

                 for this version.

        Note3: Oracle 12.2.0.x is out of support as of Jan-2022 and no additional patches are

                 posted for this version.

        KB Article ID# PL8694105

        Contents

        SummaryDetails

        Associated Components

        Reporting and Analytics