Solid Edge 2023 Update 0002 Announcement

2023-01-23T16:14:15Z

Summary


Details

January 23, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0002 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0002

Version: 2210.0002.004 x64

Download Solid Edge 2023 (v2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===API===

PR 10520894: Automation oOccs.AddByFilename is not honoring the "flexible hose" settings

===Assembly===

PR 10453306: Fastener System all lengths of screws in selection mask

PR 10475009: Designed/simplified Assemblies holding the control key

PR 10498442: Unable to create a simulation report for an assembly that contains a weld

PR 8633765: Chain selection for Tube in XpresRoute not working for 2D Sketches

PR 8648840: Crash when using replace function

===Draft===

PR 8669655: Random crash when updating drawing

===General===

PR 8648335: Orientation keys are not working on the first attempt for Coincident Plane

===Part/Profile/Sheetmetal===

PR 10507303: Add/Cut direction issue

PR 10505018: Hole Saved Settings list is missing from the VCB in Ordered mode

PR 8641346: Equation Driven Curve does not consider Units from Variable Table

PR 8653590: Quick Pick makes Solid Edge Crash

===SEEC===

PR 10504433: Unable to run ATT, ATTi and SESE with a SolidEdgeClassicPlus license

PR 10221766: Replace Revision does not work correct with Multiple Revisions enabled

PR 10501931: Part occurrences are being replaced in assembly

PR 10472528: Revise through Structure Editor creates Multiple Datasets

===TechPub===

PR 10419516: Tech Publication Export to PDF/HTML will not render end line in table

PR 10453057: Some illustrations are not "remembered" when document is saved and closed

===2D Nesting===

PR 8618657: License Borrow does not work in 2D Nesting

KB Article ID# PL8694100

Contents

SummaryDetails

Associated Components