Where is the NX Structure Designer Library Install tool?

2023-01-16T10:40:29Z

Summary


Details

In NX 2206 and earlier the tool for installing the NX Structure Designer Library in Teamcenter was found in the folder %UGII_BASE_DIR%\NXSTRUCTUREDESIGN\InstallationTool\StructureDesignerLibraryInstallation

For example:C:\Program Files\Siemens\NX2206\NXSTRUCTUREDESIGN\InstallationTool\StructureDesignerLibraryInstallation

The tool could be run by modifying and executing Structure_Design_Library-Installation.bat.  Full instructions for using this are provided in accompanying document Instruction_StructureDesigner_Library_Installation_vN.0.docx.

In NX2212 and later this folder and installation tool are no longer present. Where is this tool and how can the NX Structure Designer library be installed?

Solution

The import tool has been updated in NX2212 to include additional options and to support the import of multiple libraries types.  Consequently it has been moved a new location which is: %UGII_BASE_DIR%\DESIGN_TOOLS\library_installation.

For Example:
C:\Program Files\Siemens\NX2212\DESIGN_TOOLS\library_installation

To install the library, run the file nx_library_installation.exe from a location where you have write access.

The type of library being installed can be selected in the Library Configuration Step. 


Other libraries that can be installed with this tool are:
- Ship Structure Library
- NX Mechatronics Reuse Library
- BIM Design Library
- NX Diagramming Library

KB Article ID# PL8692760

Contents

SummaryDetails

Associated Components