Sketch not internalized when creating a contour flange

2023-01-12T07:08:35Z

Summary


Details

Even though using existing sketch curve to create a (base) contour flange, the sketch curve is not internalized.

It's even though setting "Make Sketch Internal to Child Feature" in "Modeling" preference.

Reproduced Steps:

1. Create a sketch curve


2. File > “Preferences” > “Modeling” > General > Behavior

  -1. Toggle “Make Sketch Internal to Child Feature” ON


3. Go to Sheet Metal application > Counter Flange


Result : Sketch not internalized


Solution

The behavior is due to NX bug and will be fixed in NX 2306 Series.

Workaround : Explicitly execute “Make Sketch Internal” after creating the counter flange.

Notes

This issue occurs in NX 2212 Series and lower.

***Please refer to PL8691932 for Japanese article.

Release Versions
  • NX V2212
Platforms
  • Windows x64 10

KB Article ID# PL8691933

Contents

SummaryDetails

Associated Components