NX NX does not start in native language / UGII_LANG is ignored Deutsch German French Francais Spanish Espanol Italian Italiano Sprache Menu Userinterface

2024-06-17T12:05:20Z
NX System Administration

Summary


Details

UGII_LANG is set to start NX with GERMAN, FRENCH, SPANISH etc. user interface / menus, but NX stays in English.

Solution

Since NX 2212 there was a change in the localization:

[from nx_install_wnt.pdf]

Please use use this option when installing to avoid the issue:

[Setting in question to have the native language menus installed]

This option can be update, too, when using the change option from "Add or Remove Programms" from within Windows.

KB Article ID# PL8691759

Contents

SummaryDetails

Associated Components

Installation