Unable to select objects in IGES export.

2023-01-11T01:33:29Z

Summary


Details

In Assembly environment, when exporting IGES after making one component Work Part, unable to select objects even though trying to select them using "Selected Objects".

Reproduced Steps:

1. Create an assembly structure and its components

2. Make one component work part

3.  File > “Export” > “IGES” > “Data to Export”

  -1. As “Export” of “Model Data, choose “Selected Objects” from the pulldown list

 -2. Select objects in Graphic


Solution

The behavior was due to NX bug and has been fixed in NX 2007 Series.

Workaround : Working Top Assembly work part and perform IGES Export.

Notes

The issue is occurring in NX Series from NX 1926 to NX 1980.

***Please refer to PL8691678 for Japanese article.

Release Versions
  • NX V2000
Platforms
  • Windows x64 10

KB Article ID# PL8691679

Contents

SummaryDetails

Associated Components