NX Unable to enter PMI angle and chamfer dimensions for conical face

2023-01-12T06:56:19Z
NX for Design

Summary


Details

Able to create PMI angular and chamfer dimensions for planar faces, but not for conical faces. (not allow even to select.)

Reproduced Steps:

1. Create a cylindrical solid and a chamfer


2. Try to create PMI angle and chamfer dimension


Solution

The behavior was working as designed and there were some design limitation to cylindrical and conical shapes, but it has been enhanced/implemented. The following NX versions have been improved to allow selection and input of cylindrical and conical faces.

Angular Dimension : NX 2206 Series

Chamfer Dimension:NX 2212 Series


Workaround:

By modeling 3D shape, such as the lines, create PMI angular dimension for it.

Notes

Angular Dimension(What’s New in NX 2206)

https://docs.sw.siemens.com/ja-JP/doc/209349590/PL20200605195244930.whatsnew/xid2055186

Chamfer Dimension(What’s New in NX 2212)

https://docs.sw.siemens.com/ja-JP/doc/209349590/PL20220512394070742.whatsnew/xid2105059_v1

***Please refer to PL8691651 for Japanese article.

Release Versions
  • NX V1953
Platforms
  • Windows x64 10

KB Article ID# PL8691653

Contents

SummaryDetails

Associated Components

PMI