The input fields of the x and y coordinates are grayed out while using the 'Move' command.

2023-01-10T16:34:59Z

Summary


Details

While using the 'Move' command the user is wonders why the input fields of the x and y coordinates are shown grayed out and are not usable for an input of specific values.

The input fields of the x and y coordinates are shown grayed out while using the 'Move' command

Solution

This happens if the 'Snap to Grid' option is toggled ON.

'Snap to Grid' toggled ON means the x and y input fields are unavailable

If the 'Snap to Grid' option will be toggled OFF the input fields are available for an input again.

'Snap to Grid' toggled OFF means the x and y input fields are available

KB Article ID# PL8691346

Contents

SummaryDetails

Associated Components