- tcin_template_setup fails to import templates.
- Errors output to screen show
D:\apps\share\nx\nx2206\UGII\templates\sample> tcin_template_setup.bat -u=infodba -p=infodba -g=dba
**** Doing NXDM template import:
"C:\Users\..\AppData\Local\Temp\templates\tcin_import.exe" -u=infodba -p=infodba -g=dba -publish_i=yes -default_t="Item" -dir="C:\Users\..\AppData\Local\Temp\templates" -default_a=new_revision -default_n=autotranslate -default_f=infodba:"NX Templates" -s=nxdm_template_import.clone"
Starting import operation...
FCC interface version fms.13.3.20220108.00.
Loaded implementation library '..\tccs\lib\FCCClientProxyDllv16064.dll'.
FCC Interface Implementation fms.14.2.20221104.00 initialized.
***** import operation failed
- NX syslog shows
*** EXCEPTION: Error code 940757 in line 357 of o:\nx2206\ip1700\src\pdmservices\no\ind\PDM_Services_StartupService.cxx ...
+++ NX cannot be started as NX Foundation( NX0TCIN ) database feature is not installed in Teamcenter database.
- After installing the feature in TEM,
tcin_template_setup.bat succeeded.