RobotExpert Controllers for ABB_RAPID, DEFAULT, KUKA_KRC, YASKAWA_INFORM

2022-12-27T07:23:32Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that RobotExpert controllers for "ABB_RAPID, DEFAULT, KUKA_KRC, YASKAWA_INFORM"

are available for download from https://support.sw.siemens.com.

See RobotExpert_Controller_Name_changes_log.htm for details concerning this update.

Note: This file is located in the 'OLP Change Logs' folder directly under the 'RobotExpert Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select 'Additional Downloads'

- Select 'RobotExpert Robot Controllers'

- Select 15.1, 15.1.2, 16.0, 16.1, 16.1.1, 16.1.2 or 17.0

Download the file(s):

RobotExpert_15.1_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_15.1_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_15.1_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_15.1_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_15.1.2_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_15.1.2_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_15.1.2_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_15.1.2_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_16.0_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_16.0_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_16.0_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_16.0_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_16.1_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_16.1_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_16.1_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_16.1_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_16.1.1_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_16.1.1_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_16.1.1_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_16.1.1_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_16.1.2_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_16.1.2_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_16.1.2_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_16.1.2_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

RobotExpert_17.0_ABB_RAPID_64BIT_v5.11_23_12_2022.exe

RobotExpert_17.0_DEFAULT_64BIT_v2.109_23_12_2022.exe

RobotExpert_17.0_KUKA_KRC_64BIT_v5.17.1_23_12_2022.exe

RobotExpert_17.0_YASKAWA_INFORM_64BIT_v6.34.1_23_12_2022.exe

To Install:

Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the RobotExpert installation).

Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8690201

Contents

SummaryDetails

Associated Components