NX How to check whether the installed fonts are for all users or specific users

2022-12-24T15:13:21Z
NX for Design

Summary


Details

How to check whether the installed fonts are for all users or specific users.

Solution

If you selected “Install for all users” while installing fonts, in the properties of the fonts it shows the location is shown as c:\Windows\Fonts.

Refer to the below screenshot for more info.


If used option "install" only it installs fonts installed user-specific.  these fonts can be displayed in the Note dialog box.


KB Article ID# PL8690112

Contents

SummaryDetails

Associated Components

Drafting