Until SE2022, the theme selection dialog of the attached image was displayed at the first startup.
Is this dialog removed in Solid Edge 2023?
Now user cannot find any themes other than "Balance" among the themes that were prepared from the time of installation. Was all it removed?
SolutionSolid Edge 2023 only delivers a single theme — "Balanced" — with the other two gone.
We do not recommend using the themes from an older version with Solid Edge 2023 since the options and layouts may not work.
Notes8622621