Solid Edge 2022 - Maintenance Pack 11 Announcement

2022-12-19T13:35:30Z

Summary


Details

December 19, 2022

Dear Solid Edge Customer:

Solid Edge 2022 Maintenance Pack 11 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2022 MP11

Version: 222.00.11.02

Solid Edge 2022 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

Support Center: https://support.sw.siemens.com

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Maintenance Packs, navigate to your Support Center profile:

https://account.sw.siemens.com/profile, scroll down to Newsletter Subscriptions, then check the box for

Software Field Bulletin. 

============================================

This Maintenance Pack addresses the following PRs:

============================================

===API===

PR 224993: Added new APIs to control the placement of adjustable Assembly and tubes

===Assembly===

PR 10327602: Software crash on Simplify Assembly

PR 10386139: Search and replace did not always show parts that were overridden

PR 10465397: Simplify with Visible Faces command fails

PR 10477532: Pipes did not pull in parent part face styles

PR 10488357: Reorder is slow when multiple occurrences are selected

PR 10500036: User not able to mirror/pattern Material addition features

PR 10419827: Escape key doesn't Finish sketch command in Assembly

PR 10438783: Adjustable Tubes are not staying on paths

PR 10460398: Copy of a component with Mate containing Range values ending up at the wrong position

PR 10461216: Wrong physical properties if "in place editing" subassemblies

PR 10492211: Bad start performance of pathfinder/Standard Parts

PR 10500461: Pipes do not show up in the correct length when parts are made inactive

PR 10502176: Selecting inactive parts in [Match Coordinate Systems] results in an error

PR 8621544: Crash in GeomInspector in V222MP10

PR 8615893: Pathfinder contents disappear after selecting multiple items when "auto-scroll to selected part" is set

===Draft===

PR 10224669: Alternate position settings get lost on drawing views, although inactive

PR 10499968: Weld symbol - identification line is wrong, has to be dashed, regression

PR 10466636: Offset 2D cause Solid Edge to freeze

PR 10517082: Solid Edge shuts down when using Edge Painter

===General===

PR 10377203: Random aborts when Windows 'Use text cursor' setting is "On".

PR 10484530: Can't select any surfaces with the "define" command in Simulation

===Part/Profile/Sheetmetal===

PR 10460889: Cannot edit tangency on a 3D curve (3D sketch) - SE will crash

PR 10488476: "Part Painter" - Resetting face colors after five selections

PR 10472052: Existing custom properties are overwritten by the exposure of variables

===SEEC===

PR 10393277: Import of second draft file overwrites existing dataset in Teamcenter.

PR 10480893: FOP members cannot be replaced by a new revision.

PR 10504433: Unable to run ATT, ATTI, and SESE with a SolidEdgeClassicPlus license

===Translators===

PR 10441588: IFC Import generates incorrect data

PR 10442368: Inventor Data Migration Error

PR 10502339: DWG translation fails

KB Article ID# PL8689366

Contents

SummaryDetails

Associated Components