Tecnomatix Is there any license required, if user install the virtual reality client and participate in VR session as a guest ?

2022-12-19T12:34:00Z
Process Simulate

Summary


Details

Application :

Tecnomatix 17.0

Process Simulate (VR)

Query :

If user install the virtual reality client application and participate in VR session as a guest then, is there any license required?
It is assumed that multiple people will participate in the session by using the head-mounted display of the VIVE system for one host terminal of the VR session.

Solution

As per the VR collaboration documentation:
"Process Simulate users can invite others to collaborate in a virtual reality session, even those who do not run Process Simulate."

This implies that there is any license requirement for these users.
If you observe any issues while collaborating, you can always reach out to us.

Additional information for the number of users who can connect (as per R&D) :

We're not aware of any limitations in terms of a maximum value for parameter MaxConnections (given in file NetworkConfiguration.xml located at eMPower\VR\Config).
Note that performance may be impacted with a large number of connections, depending of course on the quality of the network.

KB Article ID# PL8689353

Contents

SummaryDetails

Associated Components

Process Simulate Collaborate