About "Pitch Angle" option of the 'Hood Visibility Line' command

2022-12-23T11:00:47Z

Summary


Details

In 'Vehicle Design Automation' application there is command 'Hood Visibility Line'.

In 'Hood Visibility Line' dialog there is option 'Pitch Angle' and it has a value.

What is the meaning of this value?

Solution

The 'Hood Visibility Line' function uses a series of section planes to generate the hood visibility line. Pitch Angle is used to specify the section plane interval value that is used to calculate the number of section planes sampled in the range from -90 to 90 degrees.

KB Article ID# PL8688300

Contents

SummaryDetails

Associated Components