PMI Standard for 3D dimensioning

2023-02-24T11:54:52Z

Summary


Details

What are the standards for Solid Edge PMI?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V223.0
Solution

The 3D ISO standard is ISO 16792.

The ANSI standard is ANSI/ASME Y 14.41.

These standards describe representation in 3D.  They do not go into all of the details of general dimensions and annotations - that is covered in other standards. An example would be ISO 129 which is the General Principals of Dimensioning and Tolerancing.

Notes

KB Article ID# PL8688267

Contents

SummaryDetails

Associated Components