How to customize the behavior on Save for UGPART dataset.

2022-12-23T10:42:18Z

Summary


Details

How to customize the behavior on Save for UGPART dataset so that predefined Save Actions should be performed on UGPART dataset.(like as in UGMASTER dataset)

The user has configured TC_NX_CM_automatedDecision_Actions as below.


Now when a UGPART dataset is not checked-out, they want user to check out the data explicitly before modifying it. Therefore if the data is not checked out, they do not want to show “Save” in the selectable actions on Save dialog.

But this can be achieved in case of UGMASTER dataset, where as in case of UGPART dataset the default save action is shown as "Save" only.

Solution

The customization of the Save management dialog is not supported for the UGPART dataset.

Since non-master drawings cannot be "saved as" or revised, so we cannot show those actions here.

UGMASTER being the primary dataset we support save as and revise which is performed on the item revision and so those options make sense for the master part.

We wanted to keep the original save behavior in case of non-master, which is why save is the default action.

If the user selects ignore once, next time in session it will be remembered for that drawing and it will be ignored by default.

KB Article ID# PL8687861

Contents

SummaryDetails

Associated Components