Automatic Connector and Meshing in Simulation fails

2023-04-03T15:44:16Z

Summary


Details

The customer has client machines where it is not possible to use the 'Automatic Connector' in Solid Edge Simulation - they will get the message "No connections found".

Meshing also fails with a Nastran error.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V221MP12
Solution

This is often caused by permission issues.

Please try the following:

-Point the scratch folder, e.g. "C:/SESim_scratch". Make sure you have space and permissions in the folder.

-Start Solid Edge once with 'RMB/run as admin'.  In "[C:\Program](file:///C:/Program) Files\Siemens\Solid Edge 2023\Simulation\x64 run "femapapi.exe".

Notes

KB Article ID# PL8687303

Contents

SummaryDetails

Associated Components