Solid Edge Solid Edge Version 2210 - is this a new versioning system?

2023-04-03T15:58:59Z
PART/SHEETMETAL

Summary


Details

In Solid Edge 2023, I see reference to the version as 2210.  What does this mean?

Platforms
  • INTL64 windows-1064
Release Versions
  • Solid Edge V223.0
Solution

This can be found in the Solid Edge documentation:

https://docs.sw.siemens.com/en-US/doc/246738425/PL20211001099989437.newse/xid2081615

New Solid Edge version format

=============================

As a part of the initiative to align various products in the Digital Industry Software (DISW) portfolio and maintain consistent release numbering, Solid Edge version information is using a new format. For example, Version 2210.0003.The version is displayed in the form of YYMM.0000 where YY is the year of the software release (22), MM is the month of the release (10), and the last two digits indicate the maintenance update. In this example, the software release is October 2022 and the maintenance update is 03.

Notes

KB Article ID# PL8686150

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES