Unable to export contour flange

2022-12-08T20:39:24Z

Summary


Details

When trying to export a solid with a contour flange using the "Export Part" function, an error is output and the export fails.

Reproduced Steps:

1. Create a SB Tab and SB Secondary Contour Flange


2. File > Export > Part

   -1. Feature Parameters = Retain Internal or Retain All Parameters

   -2. Other options are OK for reproducing


Solution

The behavior is due to NX problem and will be fixed in NX 2306.

Workaround: Perform 1 or 2 below.

1. Specify "Remove Parameter" in "Feature Parameters" during exporting.


2. use other export commands such as Parasolid.

Notes

This problem has been occurred since NX 1899.

Occurrence condition : Export bodies with SB Secondary Contour Flange features. (This problem does not occur with SB Base Contour Flange.)

***Please refer to PL8686075 for Japanese article.

Release Versions
  • NX V2206
Platforms
  • Windows x64 10

KB Article ID# PL8686076

Contents

SummaryDetails

Associated Components