Unable to save "Check Wall Thickness" analysis

2022-12-07T23:54:14Z

Summary


Details

”Check Wall Thickness” can save only one result for solid body analysis. Depending on the design workflow, I would like to change the thickness range, other options and save some results. It is possible to change the settings and display the results each time, but it is very time-consuming. Is there a way to save multiple results?

Reproduced Steps:

1. Menu > “Analysis” > “Molded Part Validation” > “Check Wall Thickness”

2. “Calculate” tab > select body > select “Calculate Thickness” button > select Save Results > OK

3. Repeat Step 1 and 2 with changing some options

*** "Wall Thickness Analysis" is saved in the part navigator, but only one result can be saved.


Solution

The behavior is working as expected, but the functionality is enhanced to save multiple results on NX 2212 Series.

Notes

Please see NX 2212 What’s New guide for more information.

** NX 2212 series is scheduled to be released in December 2022.

***Please refer to PL8686043 for Japanese article.

Release Versions
  • NX V1926
Platforms
  • Windows x64 10

KB Article ID# PL8686044

Contents

SummaryDetails

Associated Components