Unable to import multiple Parasolid at the same time

2024-08-05T23:35:39Z

Summary


Details

Multiple Parasolid files are unable to select in Parasolid Import command. It can be selected only one in the import dialogue.

Reproduced Steps:

Open New part

“File” > “Import” > Parasolid

Select a button to specify the Parasolid



Solution

The behavior is working as expected. It's due to the design change so that only one file can be selected in "Import" command of NX 2007 Series.

Notes

Up to NX 1980, multiple Parasolid files could be selected, but in the process of enhancing NX integration function when importing Parasolid files in NX 2007, the design was changed so that multiple selection is not possible due to the limitation.

Reference: The behavior in NX 1980.


***Please refer to PL8685915 for Japanese article.

Release Versions
  • NX V2015
Platforms
  • Windows x64 10

KB Article ID# PL8685918

Contents

SummaryDetails

Associated Components