NX NX Structure Designer Templates are not getting imported into Teamcenter (4 - Tier)

2022-12-23T11:22:28Z
NX for Design

Summary


Details

NX Structure Designer Templates are not getting imported into Teamcenter (4 - Tier)

Import was successful but received PAX error when placing the structure.

Platforms
  • na windows-1064
Release Versions
  • NX V2019
Solution

we need to add a structure designer PAX file to the preference:

The PAX is not read from the local machine once the below preference is set.

TC_NX_FileNewPAXFiles_NX2027=CustomerItem/A

nxdm_ugs_structure_design_templates/AIn the same order as above, both the pax files are read and the templates within are made available for the user.

Notes

KB Article ID# PL8685904

Contents

SummaryDetails

Associated Components

Modeling Structure Designer