Solid Edge Solid Edge Electrical - Naming Convention

2022-11-29T17:29:36Z
APPLICATION

Summary


Details

How to change default wire name?

Currently, the default name is "WIRE #". Would like to change it to use an ANSI/ISO standard.

Platforms
  • na windows-1032
Release Versions
  • Solid Edge V222.0
Solution

Under the Project dropdown menu, select Default Naming...

First, open a Project but do not open any Diagrams.


 When you change the default name and apply it, it will change all existing wires, and any new ones that are placed.

Notes

KB Article ID# PL8685477

Contents

SummaryDetails

Associated Components

APPLICATION: SE_ELECTRICAL