Tecnomatix XML PARSING ERROR WHEN SAVING TO EMSERVER IN PROCESS SIMULATE

2022-11-23T15:25:20Z
eM-Server

Summary


Details

There is a Process Simulate user who cannot save his study to the eM-Server. He keeps getting the following error. He has tried to restart his laptop.


"The file is not valid for the following reasons: XML parsing error: 'A security package specific error occurred,'. line number 1. Column =0"

Platforms
  • na windows-1064
Release Versions
  • Tecnomatix V15.1
Solution

Please create/change the value of the following registry key on the Windows Server machine:

[HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Policies\System\Kerberos\Parameters]"supportedencryptiontypes"=dword:7ffffff8

This is the non-working value.

"supportedencryptiontypes"=dword:7ffffffc

This is the value that works.

After adding/correcting the value, the server must be rebooted for the new value to go into effect.

Notes

https://scomblogs.com/f/a-security-package-specific-error-occurred---runbook-designer

https://communities.vmware.com/t5/VMware-PowerCLI-Discussions/connect-viserver-not-passing-thru-user-credentials-in-Windows/td-p/1391755

KB Article ID# PL8684668

Contents

SummaryDetails

Associated Components

eM-Server