How can the width of a "Curve by Table" line be changed?

2022-11-21T21:44:17Z

Summary


Details

The width of a "Curve by Table" created line is too wide.
How can the curve width be adjusted? 

Solution

The "Curve by Table" line width is controlled by the Width Setting in the Curve Default Face Style.

To change the width open the Styles Dialog located in the View Tab in the Style Area.

Solid Edge View Tab

Select Face Styles and from the Styles list, choose Curve Default and click Modify.

Solid Edge Style Dialog

Open in the upcoming Modify Face Styles dialog the Edges Tab, change the Width setting to a value needed, The default value is "3", confirm the modification with OK or Apply

Solid Edge Modify Face Styles Dialog 

Confirm with Apply to close the Styles dialog.

The change is reflected at existing "Curve by Table" Lines and will be used now for the line creation in the file.

Notes

As this setting is file dependent, it is suggested to set this width value in a Solid Edge file template to get it as default setting for future use in new files.

Visit our on-line Documentation to learn more about "Curve by Table" curve creation and the Applying Formats with "Styles".

KB Article ID# PL8683895

Contents

SummaryDetails

Associated Components