Behavior that the same geometry can be selected multiple times by measure command

2022-11-15T03:39:41Z

Summary


Details

It's possible to select an already selected geometry multiple times in Measure command. Is this behavior intended?

Reproduced Steps:

1. Creating a box solid

2. Selecting the same geometry in "Analysis" tab > "Measure“


Solution

The behavior is working as expected.

Notes

An option to enable/disable multiple selection is added in NX 2212 Series. This makes it operable in line with designer's needs.

Reference: By making it possible to select the same object, for example, it's possible to measure the angle dimension with the center line of the cone face as shown below.


***Please refer to PL8682453 for Japanese article.

Release Versions
  • NX V2015
Platforms
  • Windows x64 10

KB Article ID# PL8682456

Contents

SummaryDetails

Associated Components