The color of parts list frame changes by DXF/DWG output

2022-11-15T03:38:46Z

Summary


Details

When opening DXF/DWG output file in AutoCAD, the color of one part of the frame are changed.

Steps to reproduce:

1. Prepare an assembly and Parts List in drawing


2. File > Export > AutoCAD DXF/DWG

*** The issue occurs any option.

3. Load the data output by AutoCAD (or from the NX side, File > Open)


Reference:


Solution

The behavior is due to NX problem and is fixed in NX 2212 Series.

Workaround :

There is no workaround on the NX side. Please change it by imported software such as AutoCAD.

Notes

The issue occurs in both of DXF and DWG.

The issue occurs in NX 1899 Series and higher.

***Please refer to PL8682450 for Japanese article.

Release Versions
  • NX V2015
Platforms
  • Windows x64 10

KB Article ID# PL8682452

Contents

SummaryDetails

Associated Components