PMI balloon notes resize to unintended size

2022-11-14T23:07:16Z

Summary


Details

After copy/paste PMI Balloon Note, expanded or reduced the graphic window. And then executing the "Resize" command, the balloon becomes an unexpected size.

Steps to reproduce:

1. Create a simple model and some PMI Balloon Note


2. Copy and paste one PMI Balloon Note


3. Zoom in or out on the model view

4. “PMI” > “Resize”


Solution

This behavior is due to a design limitation of "PMI Balloon Note", and if you "Resize" the copied/pasted balloon, you will get unintended results.

Workaround:

Create new PMI Balloon Note without using copy/paste of PMI Balloon Note.

Notes

***Please refer to PL8682334 for Japanese article.

Release Versions
  • NX V1973
Platforms
  • Windows x64 10

KB Article ID# PL8682335

Contents

SummaryDetails

Associated Components