When exporting TDP, attributes other than the top level are exported to "automatic table"

2022-11-14T23:05:21Z

Summary


Details

In the template part for 3D PDF output, components other than the top level are exported even though the attribute is defined in "Automatic Table" and the output range is set to "Top level Only".

Reproduced steps:

1. Preparing the template part (PMI > New Template) and Save it

  -1. For example, define CALLOUT (Product number) attribute

  -2. Select "Top Level Only" as "Scope"


2. Preparing an assembly model( such as below)


3. PMI tab > Publish

  -1. Select the template created in step 1

  -2. Other settings are as desired

4.  Open the output PDF with Acrobat Reader or etc.


Solution

The behavior is due to NX problem and will be fixed in NX 2306.

Notes

The behavior is :

         - also occurs when using the JT Plus PDF template.

         - occurs in all series from NX 1953 series to NX 2206.

***Please refer to PL8682233 for Japanese article.

Release Versions
  • NX V1980
Platforms
  • Windows x64 10

KB Article ID# PL8682234

Contents

SummaryDetails

Associated Components