Solid Edge SSA-258115: DWG File Parsing Vulnerability in Solid Edge 2022 thru MP8

2022-11-03T15:48:43Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

Updated: 3-NOV-2022

SOLID_EDGE

SSA-258115: DWG File Parsing Vulnerability in Solid Edge 2022 thru MP8

As outlined in the Siemens Product Certification team's security report SSA-258115, a small vulnerability resulting from a manually derived, malicious file manipulation could be triggered when the application reads files in a DWG file format. If a user is tricked into opening a malicious file with the affected application, this could lead to a crash and potentially arbitrary code execution.    

Please Note: There have been no actual reported customer cases associated with these vulnerabilities.    

If the recommended solution/remediation documented in the Siemens Product Certification security report (SSA-258115) is implemented, this vulnerability will be eliminated.

The worst-case outcome in these scenarios is the same as the worst-case for any phishing attack. You are vulnerable to ransomware, loss of IP, loss of personal information, or general exposure of data on your system or network.

As always, we encourage customers to provide appropriate network protections, utilize the concept of "defense-in-depth," and don't open files from unknown or untrusted sources. 

Hardware/Software Configuration

Product: SOLID_EDGE

Affected Software: Solid Edge 2022 thru MP8

KB Article ID# PL8681707

Contents

SummaryDetails

Associated Components

SE_BETA