NX Duplicate sheet letters and zone numbers displayed after deleting Drafting sheet.

2023-01-09T14:35:31Z
NX for Design

Summary


Details

After deleting a drafting sheet, the existing sheet shows duplicate sheet letters and zone numbers. Why?

Platforms
  • INTL64 windows-1064
Release Versions
  • NX V2007
Solution

The problem is arising because Create Labels toggle in the Borders and Zones command is checked in the template file. When this setting is turned ON, the zone notations can get recreated during an update event, most likely triggered by sheet delete edit in this case. The problem is seen when the recreated zone notations get mixed up with the ones created by user.

Unchecking Create Labels toggle should rectify the problem.


Notes

KB Article ID# PL8681507

Contents

SummaryDetails

Associated Components

Drafting