Displayed Solid Bodies are not Smooth.

2022-11-17T21:32:02Z

Summary


Details

Can the bodies displayed on the NX graphics screen be smoother?

Platforms
  • na windows-1032
Release Versions
  • NX V1973
Solution

Below are several settings that can improve model display. All of these options will reduce the computer graphics performance to different degrees.

1. When loading an Assembly make certain that the Assembly Load Options -> Scope -> Option is set to Fully Load. This setting effects the display of Components.


2. Set File -> Preferences -> Visualization -> Performance -> Accuracy -> Advanced -> Resolution -> Fine -> Align Facets Along Edges(Checked). These two settings will improve the display of any model.


3. Set the File -> Preferences -> Manufacturing -> Geometry(Tab) -> Needle Count -> Medium to a larger number to improve the display of manufacturing IPW models.


Notes

KB Article ID# PL8681339

Contents

SummaryDetails

Associated Components