"The wizard was interrupted before Tecnomatix 2206 could be completely installed."

2023-01-16T21:23:28Z

Summary


Details

Cannot install Process Simulate

After running 64bit/setup.exe it goes straight into "The wizard was interrupted before Tecnomatix 2206 could be completely installed".

Platforms
  • na windows-1064
Release Versions
  • Tecnomatix V2206
Solution

Checked installer logs at %temp%

MSIXXXXX.log at %temp% had error "1603"

(https://learn.microsoft.com/en-us/troubleshoot/windows-server/application-management/msi-installation-error-1603)

Not stated in the link, but the media location path was too long (in desktop+ additional folders).

Moved install media to a shorter path and ran fine.

Notes

KB Article ID# PL8680307

Contents

SummaryDetails

Associated Components