Solid Edge Solid Edge interface scaling when using multiple screens

2022-12-01T10:48:01Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

When working with multiple screens and the scaling option from the Windows "Scale and Layout" display settings, Solid Edge scales the interface from only the default screen.

Assuming that the basic screen is the laptop display (Full HD) and the additional screen is a 4K monitor, it is not possible to scale the Solid Edge interface. You can turn on a 4K monitor as the default screen, but in many cases it is undesirable.

Solution

Windows has an option that allows you to change the method of scaling Solid Edge: 




KB Article ID# PL8680211

Contents

SummaryDetails

Associated Components

SE_BETA