Active Workspace Open in Solid Edge command not available

2023-01-13T10:20:27Z

Summary


Details

I am using Teamcenter 14.1.0.1 with AW6.1.1 and Solid Edge 2023

I have started Active Workspace (AW) from Solid Edge.  When I open an assembly in AW it opens in Structure Manager. The Open in Solid Edge command is only available if I open the 'Attachment' tab and select the dataset.

This is very annoying if I am using the tree view.  I have to change the view to Tree with summary, then go to the summary tab and select the dataset.

I have installed MCAD Integration but it does not solved this issue.  Is it possible to make this command available in the Structure Manager Tree view?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V223.0
Solution

Run the ..\aw2\stage\awbuild.cmd in a Teamcenter command prompt:

  1. Open a Teamcenter command prompt.
    1. Change current directory to Active Workspace Client installation staging directory.

      e.g. cd ..\aws2\stage

      3.  There will be some *.zip files will in sub folder “out”.  Make a backup of the files (DO NOT FORGET TO DO THIS).

      4. Run the awbuild.cmd from TC command prompt.

      This utility will publish the new content to the gateway.

      Notes

      KB Article ID# PL8679925

      Contents

      SummaryDetails

      Associated Components