Solid Edge Simulation cannot Mesh - no window shows

2023-01-18T17:21:06Z
SIMULATION

Summary


Details

When the customer tries to use the Mesh command, the cursor indicates that it is loading but the command continues as if it had never been clicked.  There is no error screen.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V222MP10
Solution

First, check the path and permissions to the Nastran folder in the Solid Edge options.  Then start Solid Edge with Administrator permissions.  After this Solid Edge can be run with regular User permissions.  

If the above does not resolve the problem, run the "femapapi.exe" located in the following file path:

"C:\Program Files\Siemens\Solid Edge 2023\Simulation\x64"

Notes

KB Article ID# PL8679576

Contents

SummaryDetails

Associated Components

SIMULATION: ALL