NX Unable to correct print or plot Drawing.

2022-10-26T18:21:06Z
NX System Administration

Summary


Details

Unable to Correctly Print or Plot Complete Drawing .

Release Versions
  • NX V2027
Solution

NX2027

The reason the Print or Plot of the entire Drawing failed was due to Drawing sheet and border is outside and beyond the left side of the sheets boundary.

The lower left boundary corner is the absolute point in NX (drawings all reside within the 1st quadrant) and everything in this drawing must be moved so the focal point is the lower corner of the boundary and drawing which must be aligned. 

Only then can the drawing boundary be reduced to the correct matching Height and Length and this it will Plot correctly.

Notes

KB Article ID# PL8679228

Contents

SummaryDetails

Associated Components

Plotting