NX About TCPM Output settings in sim15_millturn_9ax_fanuc.psc in NX2027

2023-01-31T11:09:36Z
NX for Manufacturing

Summary


Details

The machining position is shifted to wrong position when running Machine Code Based Simulation on Sim 15 with the Fanuc Postprocessor.

In Post Configurator, if you change TCPM Mode to "G43.4" in TCPM Output and change G43.4 Mode to "Fix on Machine", this problem occurs.

TCPM Output Settings changed in Post Configurator

Tool Position is wrong due to the change in TCPM Setting.

Solution

You need to add a standard command in the ini file to make this work.

Please add #19696=32 to the Ini Programs like the image below.


KB Article ID# PL8679044

Contents

SummaryDetails

Associated Components

Manufacturing ISV