Can the Configuration of a CAM Part be Changed after it is set

2022-11-21T21:00:45Z

Summary


Details

File -> New -> Manufacturing is used to create a new CAM assembly. The Prismatic Milling and Hole Making template is selected which causes the cam_prismatic.dat  configuration to be set in the assembly. Once this configuration is set it cannot be changed, though. 


  The selected configuration will determine whether the user can Browse to a posted output location.   


Is it possible to override this configuration?

Platforms
  • na windows-1064
Release Versions
  • NX V1973
Solution

The configuration file can be re-selected by going to File -> Preferences -> Manufacturing -> Configuration -> Configuration File. This change will only be in effect during the current session. When the file is reopened the configuration reverts back to the configuration saved at creation.


When a new Role is created the current configuration is saved in the role. This role will override the configuration saved in the program file.


There is a Customer Default to retrieve the configuration from the role. Enabled this option to use the config saved in the role. 


Notes

KB Article ID# PL8679015

Contents

SummaryDetails

Associated Components