Solid Edge Solid Edge 2022 - Maintenance Pack 10 Announcement

2022-10-17T20:27:18Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

October 17, 2022

Dear Solid Edge Customer:

Solid Edge 2022 Maintenance Pack 10 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2022 MP10

Version: 222.00.10.03

Solid Edge 2022 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

Support Center: https://support.sw.siemens.com

Solid Edge 2022 MP Download Area: https://support.sw.siemens.com/product/246738425/download/PL20200902110958364

Note: if the MP download area URL doesn't work with your browser, please navigate from the top-level Support Center.

======================

Operating System Update:

======================

In addition to the Operating System Requirements documented in the original Solid Edge 2022 readme,

Solid Edge 2022 MP2 is now certified to run on Windows 11 Enterprise or Professional (64-bit only).

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Maintenance Packs, navigate to your Support Center profile:

https://account.sw.siemens.com/profile, scroll down to Newsletter Subscriptions, then check the box for 

Software Field Bulletin

============================================

This Maintenance Pack addresses the following PRs:

============================================

===Assembly===

PR 10450645: XpresRoute chain selection error

PR 10333529: Pipes are not positioned correctly

PR 10296594: Pipes do not show up correctly in Draft

PR 10320516: Inconsistent behavior when using FOA

PR 10364126: Deleting multiple instances of IC subassemblies

PR 10471130: Using a custom pipe results in Solid Edge close

PR 10475985: solid edge crashing while rotating assembly during SEDC Configuration process

PR 10286145: Solid Edge Exploded Distances no longer easily editable

PR 10476230: XpresRoute Piping freezes when 3D Sketch contains collinear lines

PR 10477965: The user is not able to deselect the Segment from the piping segment list

PR 10451190: aborts while saving assembly file

PR 10344008: Pipes are not correctly constrained to fittings

===Draft===

PR 10224314: Hide-All assembly feature option in Drawing view is not honored

PR 10352577: Imported Internal Components missing from Drawing Views

PR 10428523: "Update Views" tool in Drafting does not update all the views at once

PR 10462908: Bolt hole circle: error type/style line when zooming in

===Teamcenter Integration for Solid Edge===

PR 10397157: Unknown error when set / reset Read only flag of an initial saved ne

===Translators===

PR 10442368: Inventor Data Migration Error

PR 10429310: Problem with login to SE managed environment after upgrade to MP8

KB Article ID# PL8678738

Contents

SummaryDetails

Associated Components

SE_BETA