An error occurs when japanese character is specified in the DXF/DWG output file name

2022-10-20T07:15:46Z

Summary


Details

I would like to specify Japanese character for DXF file name, but a message "failed" is output to "Notification Center" in Resource bar.

Reproduced Steps:

1. Prepare a drawing sheet for DXF/DWG output

2. File > Export > AutoCAD DXF/DWG

    -1. Specify Japanese character as the output file name for DXF/DWG

    -2. Any other options are not required to reproduce the problem

3. Check "Notification Center"


Solution

The behavior occurs only in NX 2216. It’s due to NX problem, fixed in NX 2212.

Notes

1. An error is displayed in the "Notification Center", but DXF/DWG file is actually created (output) normally. please ignore the error and make use of the created data.

2. An error message is also output when Japanese characters are used in the folder name.

3. This issue occurs not only in Japanese character but in all double-byte character.

Release Versions
  • NX V2206
Platforms
  • Windows x64 10

*** Please refer to PL8678510 for Japanese article.

KB Article ID# PL8678511

Contents

SummaryDetails

Associated Components