Frame members offset

2022-12-05T16:22:36Z

Summary


Details

Frame segments are offset from the sketches to which they are applied.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V219MP4
Solution

Select the frame and edit it. Go to the Cross Section step. It will default to selecting all of the cross sections. Click the red X to deselect them, then click on just one cross section and click the checkmark to accept. Then use the arrow keys on the keyboard to move the cross section appropriately. The arrow keys correspond with the approximate direction as seen on the screen.

Notes

KB Article ID# PL8678354

Contents

SummaryDetails

Associated Components