Cannot create Simulation mesh due to the default printer

2023-01-19T14:30:06Z

Summary


Details

The customer tries to create a Mesh in Solid Edge Simulation.

Solid Edge then appears to need some time to figure out what to do but ultimately no Mesh window is shown.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V222MP9
Solution

After changing the default printer in Windows, Solid Edge will then process and the Mesh window is shown as expected. 

In Windows open 'Printer & Scanners'.

Toggle the setting 'Let windows manage my default printer' - if it ON turn it OFF and vice versa.

This is a rare fault, but changing the setting should solve the Mesh problem.

Notes

KB Article ID# PL8677422

Contents

SummaryDetails

Associated Components