How can you control the "intol/outtol" or max tool axis change in 5-axis generic motion?

2022-10-10T12:05:31Z

Summary


Details

In a generic motion operation, there are no tolerance or angular change control settings.  How can these be controlled for the path?

Solution

There is no direct tolerance specification in the generic motion operation. You can control intol and outtol by putting the operation under a machining method parent and letting it inherit the tolerances from it.  There is no specific angular control, such as the max degrees per step parameter that we have with other multiaxis operations types.

KB Article ID# PL8676833

Contents

SummaryDetails

Associated Components