Solid Edge Reference Point Cloud missing Units option

2023-01-19T09:29:24Z
ASSEMBLY PART/SHEETMETAL

Summary


Details

When opening a Point Cloud file into a Solid Edge assembly, there is no Units option available in the Command options.


If the Unit is other than meter, the geometry scales incorrectly.

Is it possible to work around this?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V222MP9
Solution

The current workaround for this is to open the Point Cloud separately in the existing scale.

Save the resulting file as a Solid Edge part, and then insert it as a Part Copy with the correct scale.

The Enhancement Request for a Point Cloud scaling option has been submitted.

Notes

KB Article ID# PL8676830

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS