NX Implemented Active Workspace and need to the NX TCIN tab back.

2023-08-01T22:09:07Z
NX for Design

Summary


Details

Teamcenter Integration tab is not available in NX after implementation of Active Workspace.

User launches NX and navigates to the TCIN tab in NX, tab is now an Active Workspace tab and user is unable to open NX files from the tab only PDF files are found.

Platforms
  • all n/a-n/a
Release Versions
  • NX V11.0.2
Solution

Set the environment variable UGII_ENABLE_TC_NAVIGATOR=true

Notes

KB Article ID# PL8676557

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX