NX Working revision limit exceeded for Item

2022-10-04T18:44:26Z
NX for Design

Summary


Details

Create an item in Teamcenter that holds no UG Master and import into Managed NX.

This raises the error "Working revision limit exceeded for Item".

Solution

The behavior is as expected.

It is observed that the revision, assigned during import, is different than the one existing in Teamcenter which was causing the revision limit to exceed.

If user want to use the existing revision ID, check if setting the customer default "Use Latest Revision when Importing into Existing Parts" helps in this case.

Notes

N/A

KB Article ID# PL8676548

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX