Extrude command missing directional vector in 2206

2022-10-26T18:21:06Z

Summary


Details

In the "Extrude" command, it was possible to reverse the direction of the extrusion.  This allowed a cube to be created and able to configure each of the corners according.

In a single "Extrude" feature it was possible to do several bodies. Using NX2206, this forces the user to create several "Extrude" features with the same result instead of in a single feature.


Solution

This Directional vector in the Extrude using a "Line" was intentionally removed in the User Interface (UI).  It can be toggled back ON with a setting in the Customer Defaults.

Customer Defaults --> Modeling --> General --> Show Section Curve Flow Direction


As you can see, this is toggled OFF by default.

KB Article ID# PL8676543

Contents

SummaryDetails

Associated Components