NX Setting Quantity Value to 2 or more in TC sets UG GEOMETRY value in NX to NO

2022-11-17T21:46:01Z
NX for Design

Summary


Details

Unable to the load data in NX.

The structure is getting loaded but the geometry is not visible in the NX  and there is a  dotted box beside it. 


This means this part is delivered to NX from Teamcenter as a Non-Geometry part. 

Select the part and go to its properties and you will see the  "Component is NON-Geometry" is toggled.   


Select the Attributes Tab in the Properties window and the UG GEOMETRY value is set to  NO.


Solution

The behavior described is a deliberate design in NX and has been in place for a long time.

Changing the quantity of a component in Teamcenter to a value other than "1" will cause the component to be marked as non-geometric when loading the parent assembly in NX.


Notes

N/A

KB Article ID# PL8676542

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX